UCI Tx sequence Window (Advanced LTE FDD Uplink)

The UCI Tx sequence window displays the currently configured UCI transmission sequence. The UCI channel cannot be transmitted in subframes occupied by UL-SCH processes. (In the Channel Setup node, set the UL-SCH State to Off, if necessary.) You can set parameters for each UCI transmission from within the UCI Tx sequence window. Click the Column Preset button to access a drop-down list that enables you to set parameters for all UCI Tx sequences to the same value. The configured parameters are displayed in the Tx Map.

UCI Tx sequence window